我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
OFS returns error 1053
Product Line
OFS

Environment
Windows 10

Resolution
When you install OFS, the following error could get get returned from the installer if .Net Framework 1.1 s not installed on the PC.
'Error 1053: The service did not respond to the start or control request in a timely fashion.
To resolve the issue, use the instructions defined in the Microsoft KB839174 (reference 'https://www.betaarchive.com/wiki/index.php/Microsoft_KB_Archive/839174'




施耐德電機Taiwan

附件
FIX_ You receive an _Error 1053_ The se...top or pause a managed Windows service.pdf [633.14 KB]