我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can I run a larger hp motor with a smaller hp softstarter ?
Issue:
Can I run a larger hp motor with a smaller hp softstarter

Product Line:
ATS48 , ATS22, ATS01

Environment:
All

Cause:
Need to up size the motor for application

Resolution;
No, it is not recommended using a smaller hp softstarter on a larger hp motor. The Softstart horsepower should match the motor and ampage should at higher than the motor rating.