我们今天能为您提供什么帮助?

How to diagnose the error when the CID file imported to IEDCT failures ?

User uses the 140NOP85000 module for IEC61850 communication, sometimes they need to import the CID file to the IEDCT and IEDCT will check the file with some rules.
If some error is reported, there will be a error log file saved by user and customer could open the errorlog file to investigate it or send it to L3 to analyse .

施耐德電機Taiwan

附件
Error.jpg [27.58 KB]