我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Are fast screws sufficient to ensure the holding of the frame of my Resi9 Electrical Panel on Trunking system?
Yes, the screws supplied with the chassis are sufficient (installed according to the description in the manual).
For more details please click on :https://www.se.com/ww/fr/FR/download/document/NHA7467001