我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How is it possible to differentiate the profiles A and E for the Harmony keys?
Have a look at the attachment which it is explained.
Actually you can find a view from the top of the key, the position of the teeth are down.
In fact the two profils are symetricals.

施耐德電機Taiwan

附件
Profile A and E.pdf [11.62 KB]