我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Which Magelis iPC will have Windows Server operating system?
Issue:
Which Magelis iPC will have Windows Server operating system?

Product Line:
HMIRSPSXR6T01, HMIRSPSXR6S01, HMIR Rack PC, Windows Server

Resolution:
From the 4/2016 catalog, only the Rack PC (HMIR) will come with Windows Server 2008 and 2012 R2.