我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How can I reset CANopen communication from a SoMachine controller to an ATV312 after an E-stop command?
Issue:
Reset CANopen communication from a SoMachine controller to an ATV312 after an E-stop command.

Product Line:
ATV312

Environment:
All using CANopen

Cause:
Reset via CANopen

Resolution:
You can use the MC_Reset_ATV FB to reset the communication after an E-Stop.