我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Are the power converters in the Field Drives de-rated like E-Flex drives?
Issue:
Are Field Drive de-rated like E-Flex drives?

Product Line:
ATV61/71 Field Drive

Environment:
De-rating the drive

Cause:
n/a

Resolution:
No, there is no de-rating on Field Drives