我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
The Function Block ETH-PORT-CTRL is not able to control the enable/disable state of FTP and HTTP.
Issue
The Function Block ETH-PORT-CTRL is not able to control the enable/disable state of FTP and HTTP.

Product Line
BMXNOE0100

Environment
Unity

Resolution
Upgrade to the BMXNOE0100 firmware version 3.0 of greter