我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the power consumption of BMXAMO0802.
Question:
Please help to confirm the power consumption of BMXAMO0802 when all 8 channels are open? 74ma or 135ma?
Since there is conflict at different publications.

Answer:
IF all 8 channels are not open and  all 8 Channels output with 20mA, the total consumption of module is around 135ma.