我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Are the ATV600 series Drives compatible with Ethernet?
Issue:
ATV600 Ethernet Modbus TCP compatibility

Product Line:
Altivar Process Drives

Environment:
All

Cause:
Installation

Resolution
Yes, Ethernet TCP/Modbus TCP is standard integrated functionality. Ethernet IP requires a separate Option Card VW3A3720 (min. Firmware ver. 1.5) or (min. Firmware ver. 1.6) VW3A3721. These are both combination TCP/IP and Ehternet IP Option Modules with dual port daisychain functionality.