我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What's the difference between reference XVUC29 and reference XVUC29P?
There are following differences:
1. XVUC29 is driven by ON/OFF signal and usually connect to relay, XVUC29P is driven by pulse signal and usually connect to PTO/PWM or transistor.
2. XVUC29 only can be changed color and mode by dip-switch, XVUC29P can be changed color and mode by input pulse signal.
3. XVUC29 supports maximum 5 layers, XVUC29P supports maximum 4 layers.
4. XVUC29 can be assembled in any layer, XVUC29P only can use under single color light unit.