我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Why do I get a Microsoft Visual C++ 2008 SP1 Redistributable package error when installing SP3.1 Webgate client for Vijeo Designer?
The Microsoft Visual C++ 2008 SP1 Redistributable package was not included with SP3.1

As a workaround you can install the SP3 webgate client file which includes Microsoft Visual C++ 2008 SP1 Redistributable package then install SP3.1.

webgate