我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
TM251MESE : Modbus TCP IOscanner channel status can be wrong
With TM251MESE firmware v4.0.4.14, when using Modbus TCP IO scanner with more than 16 channels, channels health bits may be wrong.

Firmware v4.0.5.10 (available with SoMachine v4.2) solves this issue.