我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Where to find the CAD drawings for the PM3000 Power Meter?

Issue
User needs to locate CAD drawings for the PM3000 Series Power Meter.

Product Line
PM3000 Series Power Meter

Environment
Product Documentation

Cause
CAD drawings are required for installation and design purposes.



Resolution:
The CAD drawings for the PM3000 series meter can be found on the Schneider Electric website under the Documents & Downloads section at the following link: PowerLogic PM3000 Series