我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How many Modbus RTU server devices can be connected to an HMIGTO
Issue:
Looking for specifications on how many Modbus RTU server devices can be connected to an HMIGTO

Product LIne:
Harmony, Mageils, HMIGTO, HMIGTU, HMISTU, XBTGT, XBTGK, HMIGK

Resolution:
The maximum number of Modbus RTU server devices that can be connected to a Magelis HMIGTO is 32.

The RS-485 communication cable has to be shielded and terminated properly and the maximum distance between devices is 100ft.