我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What software is used to program Magelis HMIGXU series ?

Article available in these languages: 西班牙文

Issue:
Looking to re-program a Magelis HMIGXU that came as part of a machine purchased from a company in China.

Product Line:
Vijeo Designer Basic, HMIGXU

Resolution:
Vijeo Designer Basic V1.0 or higher is used to program the Magelis HMIGXU series. This software is not sold nor supported in the North American market.

NOTE: None of the versions of Vijeo Designer do not support HMIGXU series today.