我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How configure VMWare in mode NAT and SoMachine for M251 communication via ETH 2 port
Use the following method with the VMWare configured in NAT mode:

1. Configure SoMachine the communication via "active path":

2.In the Communication Settings window , add a gateway and use the IP address of the
physique PC.

3.Select the new gateway and  Scan it

4. Now you can connect to the M251