我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What are the different ethernet racks available in M580 range ?
Issue:
What are the different ethernet racks available in M580 range ?

Product Line:
M580

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution:
M580 Ethernet racks have all the features of the X Bus racks with the addition of an Ethernet communication bus across the backplane.​

M580 Ethernet racks

All Ethernet racks are available in standard or industrially hardened versions. A hardened version has the letter H appended to the reference.