我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Will the displacement power factor on the ATV630 drive be better than the ATV61/ATV71 drives?
Issue:
Is the displacement power factor ratings on the ATV630 drive better than the ATV61/ATV71 drives?

Product Line:
ATV630

Environment:
All

Cause:
Is the power factor more efficient than an ATV 61 and ATV71 drive?

Resolution:
The displacement power factor for the ATV630 is similar to the ATV61.
See attachment for the current ATV630 and ATV930 displacement power factor ratings.

施耐德電機Taiwan

附件
Altivar Process DPF-PF_IE03draft.pdf-customer-inquiry.pdf [118.02 KB]