我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the largest SD card we can use for the HMIG3U?
Issue:
What are the specifications of the largest SD card we can use with the Magelis HMIGTO and HMIG3U?

Product Line:
HMIG3U, HMIGTO series

Resolution:
The largest SD card that can be used with the HMIGTO and HMIG3U is 32GB formatted as FAT32.