我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What should the F601 current limit parameter be set to in the ATV212 drives?
Issue:
ATV212 parameter F601 configuration

Product Line:
ATV212, S-Flex 212

Environment:
All

Cause:
What should the F601 current limit parameter be set to in the ATV212 drives?

Resolution:
The F601 Current limit parameter should be set to 110% of the Drives current rating.
Note: If you use a small size motor on a larger drive, you will need to adjust this setting to the motor FLA times 1.1.