我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is conformal coating available with the Altivar 320 drive?
Issue:
Is conformal coating available with the ATV320?

Product Line:
Altivar 320 Drives

Environment:
All serial numbers for Altivar 320 Drives

Cause:
N/A

Resolution:
Yes, the Altivar 320 come with conformal coating for increased robustness against polluted atmosphere.