我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the Fan PID function on the Altivar 600 Process Drive?
Issue:
Altivar 600 Fan PID function.

Product Line:
Altivar 600 Process Drive

Environment:
All products of Altivar 600 Process Drive

Cause:
N/A

Resolution:
The Fan PID allows the user to setup a basic PID function when the drive's Macro Configuration (Menu 7.1) is set to Generic Fan Control.
There is no difference in the parameters and the settings than when setting up a pump PID.
To access go to [Fan] - [PID controller]