我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How many Modbus/TCP client connections can you have on the M221?
Issue:
How many Modbus/TCP client connections can you have on the M221?

Product Line:
Modicon M221, Modbus server, Modbus client

Resolution:
The M221 Ethernet as a Modbus TCP Server will support a maximum of 8 Client connections.