我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Video: How do I customize the display on the Altivar Process Drive?

Article available in these languages: 芬蘭文

Issue:
How do I adjust/customize the main display on the Altivar Process Drive?

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive​

Resolution:



To adjust parameters on the top of the screen
- [My preferences] [Customization] [Param. Bar Select]

A
To adjust parameters in the middle of the startup screen
- [My preferences] [Customization] [Display Screen Type] [MPC]
C
B