我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
ATV630- How do you set up the run command on DI1?
Issue:
ATV630 set up the run command on DI1.

Product Line:
ATV630

Environment:
2-wire control

Cause:
n/a

Resolution:
Suggest to go to menu 5.5 and set 2-wire control to 2-wire and set 2-wire type to Level.  This will automatically assign DI1 to run forward.