我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the maximum motor cable length for ATV660 drives?
Issue:
Is there a recommendation for the maximum motor cable length for ATV660 drives?

Product line:
Altivar ATV660

Environment:
All

Cause:
N/A

Resolution:
150 meters with shielded cable
250 meters with unshielded cable

300 meters with shielded cable and option "300m DV/DT filter"
500 meters with unshielded cable and option "300m DV/DT filter"

施耐德電機Taiwan

附件
ATV660_Handbook_EN_NHA37111_02 cable length.pdf [140.3 KB]