我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the consequence of a simultaneous action on 2 Solo transmitters ZBRT1 ?
Considering 2 ZBRT1 paired with the same receiver (ZBRRA or ZBRRC or ...), a simultaneous action on both pushbuttons will have the following consequence:
- The gap between the simultaneous actions is less than 10 ms:
--> the orders are lost, no action on the receiver (see IS Expert EIO0000000812 page 51)
- The gap between the simultaneous actions is more than 10 ms:
A/ If the receiver is in monostable status
--> The temporisation of the output is reactivated for 500ms (see IS Expert EIO0000000812 page 55)
B/  If the receiver is in bistable status
--> The status of the receiver is changed (see IS Expert EIO0000000812 page 55)