我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Video: How to generate and configure a PUE (Power Usage Effectiveness) report in Power Monitoring Expert

Issue
How to generate and configure a PUE (Power Usage Effectiveness) report?

Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment
Generating PUE report from Web Application

Cause
User would like to know how to generate PUE report and learn how the report calculates PUE.

Resolution
A video is attached which describes a step-by-step procedure on how to generate and configure PUE reports.

Note: As of PME 9.0 the Reports tab layout looks different. However, the actual report parameters are unchanged.

PUE calculation:
PUE (Power Usage Effectiveness): The ratio between the data center and IT equipment energy measurement values.
This value is calculated for each of the required time periods by the following formula:

PUE = Sum of DataCenter Energy / Sum of IT Equipment Energy

IT Equipment – The average of the IT equipment power measurement values for each of the
time periods.

Data Center - The average of the data center power measurement values for each of the time
periods.