我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can you program the ATV320 drives' STO safety inputs from the keypad or HMI?
Issue:
ATV320 program the STO safety inputs from the keypad or HMI.

Product Line:
ATV320

Environment:
All

Cause:
Wants to know if you can program the STO safety inputs with the local keypad or remote HMI?

Resolution:
The ATV320 drives' STO functions can only be configured using the Somove software.