我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What does PWS mean on the Process Drive display?
Issue:
Customer cannot get their Process Drive to run.  Top line of the display reads status PWS.

Product line:
Altivar Process, ATV630, ATV930

Environment:
All

Cause:
SoMove connection

Resolution:
PWS indicates the drive Start/Stop is controlled by the SoMove software.  Commands to run from the external terminals or the keypad will not be taken into account.  The drive will still follow external analog signal.

施耐德電機Taiwan

附件
PWS Capture.JPG.jpg [12.57 KB]