我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Connect and change parameters on a LXM32 drive using SoMachine
Issue:
Can I connect and change parameters on LXM32 servo drive using SoMachine?

Product Line:
SoMachine

Resolution:
In SoMachine, when you add a LXM32 drive to the network, you can double click it and go to the 'Configuration of the device' tab, where you can see a SoMove-like screen (See attached).
Just like the SoMove interface, you can connect to the drive and upload/download/edit parameters.

施耐德電機Taiwan

附件
DTM.png [115.77 KB]