我们今天能为您提供什么帮助?

PlantStruxure PES: How to integrate Profibus PA instruments in PES.

Goals and Symptoms

This document is created to explain the minimum configuration for integrating Profibus PA instruments in PES.

Facts and Changes

This document has been prepared in PES Version 4.0 SP1 however same can be used in the newer versions on PES as the configuration have not been changes in latest version of PES.

Causes and Fixes

The purpose of this article is to provide guidance on how to integrate Profibus PA instruments inside PES, using PRM gateway. This article is based on a real demo platform executed in the TVDA lab with a quantum PLC and Endress Hauser instruments.

Refer to the attached document for details on configuration in PES.

施耐德電機Taiwan

附件
Integrating Profibus PA instruments in PES.pdf [1.63 MB]