我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
ATS48 soft starter can you add a time delay to the start command?
Issue:
Can you add a time delay to the start command on an ATS48?

Product Line:
Altistart 48 soft starter

Environment:
All

Cause:
Wants to set up a time delay relay.

Resolution:
You will need to add a external on delay time delay relay.