我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Does the ATV212 preset speed function override PID control?
Issue:
Overriding PID control with ATV212 preset speed function.

Product Line:
Altivar 212 ATV212

Environment:
All models

Cause:
Activation of preset speed needs to override PID control

Resolution:
The preset speed activation does not override PID control.  When activating the logic input for a preset speed, also activate a separate logic input that is assigned to 14 (PID disable) to deactivate PID control.  This way, the preset takes control.