我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can a 460V rated VFD be used in a 230V power circuit?
Issue:

Can 230V power feed a 460V rated VFD and run a 230V rated motor?

Product Line:
Altivar

Environment:
All models

Cause:
General question

Resolution:
No.  The 230V power supply is well under the specification of a 460V rated VFD.