我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is it necessary to use the Full size Neutral for the iEM330 and iEM3100 Meters?
Yes, it is necessary to use the full neutral cable (the same size as L1,L2 and L3):
1) For iEM3300, L1,L2,L3,Neutral are 50 mm2 / 1AWG;
2) For iEM3100, L1,L2,L3,Neutral are 16 mm2 / 6AWG;