我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What does the blinking COM status led mean on the ATV630 and ATV930 Process drives?

Issue:
ATV630 and ATV930 Process drives with blinking COM status led.

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Com's status LED will blink when they connect the remote HMI display to the modbus port.

Resolution:
LED will flash when the fieldbus is active and communicating.