我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Video: How can one see the last fault that occurred on an ATS48 softstarter?
Issue:
Last fault occurred on an ATS48 Softstarter

Product Line:
Altistart 48

Environment:
All

Resolution:
Go into the SUP menu and select LFt parameter.  This will display the last fault that occurred on this drive.
The previous 4 faults can be accessed through SoMove software connected to the ATS48.