我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
M241 SD card specifications
Issue:
What are the M241 SD card specifications?

Product Line:
M241

Resolution:
You can use any SD card which is an SDSC or SDHC (High Capacity), up to 32 GB maximum memory and FAT32 file system formatted.