我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
IEC or EN60204-1 compatibility for ATV600/630?
IEC 60204-1: is standard for Safety of machinery - Electrical equipment of machines – Part 1: General requirements. This gives the stop category of safety function.

On ATV630 there is STO function This safety function corresponds to an uncontrolled stop in accordance with stop category 0 of IEC 60204-1.