我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to make sure if the M580 CPU is in "No Conf" State.
M580 CPU is in "NO Conf" state if the LED Err is blinking RED in Color, LED MS and NS are blinking Green in Color.
This makes a triangle formation when we look at the CPU.

State "No Conf" means that the M580 CPU has no valid configuration stored inside its non volatile memory.