我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Does PME support the UDP protocol?
Issue
A customer would like to know if PME supports the UDP protocol.

Product Line
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x

Environment
Supported communications protocols

Cause
The User Database Protocol provides no guarantees for message delivery and the UDP layer retains no state of UDP messages once sent.
For this reason, UDP is referred to as an 'unreliable protocol' and is not suitable for real time data or historical data logs.

Resolution
UDP is not supported by PME.

施耐德電機Taiwan

探索更多
產品:
探索更多
產品: