我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What can cause an SLF1 fault on the ATV12 drives?
Issue:
SLF1 fault causes on the ATV12 drives.

Product Line:
Altivar ATV12

Environment:
All

Cause:
Interruption in communication on the Modbus network

Resolution:
• Check the connections of communication bus.
• Check the time-out (Modbus time out ttO parameter
page 83)
• Refer to the Modbus user manual