我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can we use network braking unit for Altivar ATV930 ?

Yes, there is new range of network braking units ATVRU75N4 (7.5kW unit) and ATVRD15N4 (15kW unit).
It is possible to combine up to 3 units in parallel. ATVR is compatible with Altivars: ATV320, ATV340 and ATV900.
Manual (NVE88423) and sizing tool (NVE94856) can be downloaded from schneider web.