我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Flash development toolkit FDT for Altivar drives and Windows 10/Windows11 compatibility.

Flash development toolkit FDT used for Altivar drives is compatible with Window 10 from version V4.09 release 03 and later on (win11)
Download flash development toolkit version 4.09 R03 directly from Renesas manufacturer:
https://www.renesas.com/document/swe/evaluation-software-flash-development-toolkit-v409-release-03?language=en&r=1169901
(Free registration is need on renesas).

Note: If the link is moved, use google search phrase below to find FDT v 4.09 release 03 on renesas web site
fdt v.4.09 release 03 site:renesas.com