我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can the warning message W1072 be suppressed?
Issue

An unassigned coil in a LD section leads to W1072 warning message despite checking "Nothing" for conditions which would normally result in a warning in Unity Project Settings.

Product Line

Unity pro


Resolution

In the online-help, this project setting is for EFB/DFB parameters and not for contacts and coils.