我们今天能为您提供什么帮助?

What is the difference between EF and EFB in Unity

Question:
What is the difference between EF and EFB in Unity

Answer:
Elementary functions (EF) have no internal status and one output only. If the input values are the same, the output value is the same for the executions of the function, for example the addition of two values gives the same result at every execution.
Elementary function blocks (EFB) have an internal status. If the inputs have the same values, the value on the outputs can have another value during the individual executions. For example, with a counter, the value on the output is incremented.