我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can we join two expansion cables together between BMXXBE1000 modules
Issue:
Customer needs to add an extension rack to an M340 installation using BMXXBE1000 modules. The distance between racks is around 15metres.
He wants to know if he can join two expansion cables together (e.g. BMXXBC120K & BMXXBC030K) with a standard DB9 joiner (female-female)?

Product Line:
M340, M580, BMXXBE1000

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution::
Yes, this should work, as long as the cumulative length of all the cables used in a PLC station is less than or equal to 30 m.